Why doesn't my INLINE 4
or INLINE 5 adapter work with INSITE version 5.4 or other older Cummins
software applications?
Versions of INSITE earlier than
6.3 may not be RP1210 compatible. Since the INLINE 4 and INLINE
5 adapters use the RP1210
protocol,
they will only work with software that supports the RP1210 protocol.
Visit the Compatibility pages
on this site to determine what versions of Cummins software applications
are compatible with RP1210 and the
INLINE 4 and INLINE 5 adapters.
What Windows operating
systems software will the PC driver for the INLINE 4 and INLINE 5
adapters support?
For RS-232, the INLINE 4 and INLINE
5 PC drivers support Windows™ XP,
2000, Millennium Edition, NT Service Pack 6a, and 98 Second Edition.
For USB, the INLINE 5 PC driver only supports Windows™ XP.
Will the INLINE 4 and INLINE
5 adapters work with my QuickCheck III software?
The INLINE 4 and INLINE 5 adapters
will not work with the QuickCheck III software, however,
they will work with the RP1210-compatible releases of QuickCheck
4, QuickSpec
4,
and QuickTrip
4 software
available on this site when using the optional RS-232 serial cable
to the Palm handheld. Note that you will need cable part number 3165017
to interface with the
compatible
Palm
handheld
models
listed here.
You can order this cable from your local Cummins distributor or through
the PowerStore.
Will the INLINE 4 and INLINE
5 adapters work with non-Cummins RP1210-compatible software applications?
As long as these non-Cummins software
applications are truly RP1210-compliant, the Cummins INLINE 4 and INLINE
5 adapters will work with them. However, some non-Cummins applications
have proprietary
features that make them not fully compliant with the RP1210 standard
and they will not work properly with the INLINE 4 and INLINE 5 adapters.
Test the application with an INLINE 4 or INLINE 5 adapter to verify
compatibility.
How do I download the latest
PC driver for my INLINE 4 or INLINE 5 adapter?
Go to this page and
follow the instructions to download the latest PC driver for your INLINE
4 adapter. Go to this page and
follow the instructions to download the latest PC driver for your INLINE
5 adapter. Note that the INLINE 4 driver and INLINE 5 driver
are different and you must use the correct driver for your adapter.
How do I download the latest
firmware to my INLINE 4 or INLINE 5 adapter?
Go to this page and
follow the instructions to download new firmware to your INLINE 4 adapter.
Go to this page and
follow the instructions to download new firmware to your INLINE 5 adapter.
Verify
that the version of firmware on the web page is a newer version than
what is already in your adapter, which you can find by double-clicking
on the INLINE 4/5 tray icon on your computer, before you download the
firmware. Note that you will need the Flash reprogramming utility described
below to reprogram firmware in the INLINE 4 and INLINE 5 adapters. Note
that the INLINE 4 firmware and INLINE 5 firmware are different and
you must use the correct firmware for your adapter.
How do I download the Flash
reprogramming utility for my INLINE 4 adapter?
Go to this page and
follow the instructions to download the reflash utility for your INLINE
4 adapter. Go to this page and
follow the instructions to download the reflash utility for your INLINE
5 adapter. Note that the INLINE 4 reflash software and INLINE
5 reflash software are different and you must use the correct reflash
software for your
adapter.