The QuickTrip 4 installation
is a typical Windows-based, self-executing installation. It sets up
the
application for the handheld organizer and also installs the QuickTrip
4 Conduit, which is used by the HotSync Manager to send the stored engine
data from the handheld organizer to the host PC. You must have an INLINE
4 or INLINE 5 adapter for the QuickTrip 4 application to read data.
The steps for the QuickTrip 4
software installation are listed below. It is already assumed that
you have
previously installed the handheld Desktop software. If you have not
installed this software, see the handheld handbook for instructions
on installing the Desktop software.
Download the QuickTrip 4
zip file by clicking on the button above.
Unzip the executable file using
zip/unzip software.
Click on the Windows Start
menu and click Run.
Click on the Browse button
and locate the file you have downloaded.
Click the OK button to install
the QuickTrip 4 desktop component (the Conduit), which will
also register the Palm Application with the Palm HotSync Manager.
Follow the onscreen instructions
to complete the installation. The installation places all PC components
into the root directory of the handheld organizer (typically C:\Palm
or C:\Program Files\Palm). However, QuickTrip 4 components are
placed in the \qTrip directory immediately below the Palm root directory.
Perform a HotSync operation
to install the QuickTrip 4 application on the handheld organizer.
In case of difficulties, please consult the QuickTrip 4 User's Manual.