Links Buy Online Home
Downloads:
QuickCheck 4
 

QuickCheck 4 Software Download

The QuickCheck 4 installation is a typical Windows-based, self-executing installation. The QC Configurator 4 program is included in this installation. The install program sets up the applications for the handheld organizer and also installs the QuickCheck 4 Conduit, which is used by the HotSync Manager to send the stored engine data from the handheld organizer to the host PC. You must have an INLINE 4 or INLINE 5 adapter for the QuickCheck 4 application to read data.

The steps for the QuickCheck 4 software installation are listed below. It is already assumed that you have previously installed the handheld Desktop software. If you have not installed this software, see the handheld handbook for instructions on installing the Desktop software.

  1. Download the QuickCheck 4 zip file by clicking on the button above.
  2. Unzip the executable file using zip/unzip software.
  3. Click on the Windows Start menu and click Run.
  4. Click on the Browse button and locate the file you have downloaded.
  5. Click the OK button to install the QuickCheck 4 desktop component (the Conduit), which will also register the Palm Application with the Palm HotSync Manager.
  6. Follow the onscreen instructions to complete the installation. The installation places all PC components into the root directory of the handheld organizer (typically C:\Palm or C:\Program Files\Palm). However, QuickCheck 4 and QC Configurator 4 components are placed in the \qc4 directory immediately below the Palm root directory.
  7. Perform a HotSync operation to install the QuickCheck 4 and QC Configurator 4 applications on the handheld organizer.


In case of difficulties, please consult the QuickCheck 4 or QC Configurator 4 User's Manual.

 

© 2008 Cummins Inc.