Links Buy Online Home
Compatibility:
QuickCheck
 

QuickCheck compatibility with INLINE 4 and INLINE 5

The QuickCheck 4, QuickSpec 4, and QuickTrip 4 applications are the only versions of the QuickCheck family of software that are compatible with the INLINE 4 and INLINE 5 adapters. See the chart below for Palm handheld compatibility and the basic connections needed to hook-up to the vehicle data link.

Note that QuickCheck 4, QuickSpec 4, and QuickTrip 4 are not compatible with the INLINE 5 when using the USB port of INLINE 5 adapter.

 

© 2008 Cummins Inc.