Links Buy Online Home
Compatibility:
INSITE
 

INSITE compatibility with INLINE 4 and INLINE 5

INSITE versions of 6.3A and later are compatible with the INLINE 4 and INLINE 5. Note that INSITE versions earlier than this that are not RP1210 compliant will not work with these adapters. See the chart below for an example of the basic connections needed to hook-up to the vehicle data link.

 

 

 

© 2009 Cummins Inc.